Hello Team,
Lear asked for a MCAL review (service paid by BSSM hours)
----------------------------------------------------------------------------------------
As with last review let me send you some information regarding our configuration used in order to speed up this exchange (also see MCAL configurations and other review related docs in the attachments):
Core clock configuration at max core speed with:
-Analog continous sampling non-interrupt-based of around 30 signals including external muxes (checking the result conversions in SW in a 3ms task)
-Around 40 digital signals trhough DIO.
-1 external interrupt using ICU driver and connected emios
-1 spi external device (nxp’s fs26).
-Minimum XRDC configuration without usage of HSEr
-Sleep configuration not considered as low power mode is fully in SBC FS26 hands (microcontroller powered down during low power mode).
-ASIL C compliance
-FYI using vector os
------------------------------------------------------------------------------
BR
Stefano
Hi cuongnguyenphu,
if you are able to plan for beginning next week the review with Lear pls. propose some date/time suitable for you.
Thanks and BR
Stefano
Hi @StefanoGattazzo
Let me check the input files and comeback with the estimation soon
Hi cuongnguyenphu,
is it ok next week?
BR
Stefano
Hi @StefanoGattazzo
Sorry for my late response. I was busy in the last week for other tickets.
Can we setup a meeting with LEAR on Thursday this week (22/1/2026) with your suggested time. I will arrange my schedule to join the meeting
One of my first look in the ARXML file is the mismatch between some configuration nodes that appear in only K3 RTD 3.0.0 but was removed in K3 5.0.0. For example in RTD 5.0.0 our package don't have below nodes, so it will be removed:
Could you please ask Lear to share again the latest configuration files that match with the RTD version they want to work on (RTD 5.0.0)