EB tresos AutoCore 8.8.7 for S32G3 license update 2026 didn't valid for bsw module.Dear NXP support team,
I have recently activated the new license for EB tresos AutoCore 8.8.7 as shown below:

However, after activation, BSW module generation remains disabled. The tool reports that the license is not valid for code generation.
Could you please confirm:
- Whether this license includes the required features for AUTOSAR Classic BSW code generation ?
Example

- If the license covers NXP S32G3 target support, Any steps needed to resolve this issue or provide a corrected license.
I have cross-checked the feature list between the old and new licenses. The new license (2026) is missing several features compared to the previous one, such as:
- EB_TS_OS_SUPPORT
- EB_TS_VARIANT_HANDLING
- Multiple Importer features (DBK, FIBEX, LDF, TDB)
- EB_TS_GENERATOR_PARALLEL
These features are required for AUTOSAR BSW module generation. Could you please confirm if the new license is incomplete or if an additional package is needed for full functionality?

Thank you for your assistance.
Re: EB tresos AutoCore 8.8.7 for S32G3 license update 2026 didn't valid for bsw module.Hi @chenyin_h
Additional Information,
You can import the EB AutoCore 8.8.7 simple demo RTE example located at:
C:\EB\tresos\demos\AutoCore\8.8.7-S32G399\simple_demo_rte
After the import is finished, open the configuration for any bsw module (e.g. ecuM, bswm, OS).
If the latest license is active, you will see log messages similar to the following:

Re: EB tresos AutoCore 8.8.7 for S32G3 license update 2026 didn't valid for bsw module.Hello, @khuongpham
You are welcome.
I will investigate the issue and reply you soon after any discovery found.
BR
Chenyin
Re: EB tresos AutoCore 8.8.7 for S32G3 license update 2026 didn't valid for bsw module.Dear @chenyin_h
Thank you for your response.
This use case is based on GoldVIP version 1.14, and the following packages are utilized (marked with a check symbol to indicate active usage)

This project is based on the EB AutoCore 8.8.7 simple demo RTE example located at:
C:\EB\tresos\demos\AutoCore\8.8.7-S32G399\simple_demo_rte
Additionally, several modules have been integrated from the NXP PFE Driver, CAN,UART,PORT,MCU MCAL example application:
C:\NXP\PFE-DRV_S32G_M7_MCAL_1.6.0\example_application\MasterProject_RDB3
The detail module you can see like bellow .

Could you please confirm :
- Does NXP continue to provide support license for AutoCore OS and BSW code generation as before?
- If so, what steps should I take to ensure new license ?
Thank and Br
Khuong
Re: EB tresos AutoCore 8.8.7 for S32G3 license update 2026 didn't valid for bsw module.Hello, @khuongpham
Thanks for your post
May I know if you found the issue when working with GoldVIP? If yes, which project and which version mentioned?
I will help to check it and reply you if any discovery
BR
Chenyin
Re: EB tresos AutoCore 8.8.7 for S32G3 license update 2026 didn't valid for bsw module.Hello, @khuongpham
Thanks for your sharing.
Since EB is not product of NXP, we need contact the 3rd party for checking the issues, which may take some time, I will update the status while any response received.
BR
Chenyin
Re: EB tresos AutoCore 8.8.7 for S32G3 license update 2026 didn't valid for bsw module.Hello, @khuongpham
Thanks for your patience.
It is noticed that the license has been updated, which may activate the EB Autocore correctly.
Sincerely sorry for your inconvenience.
BR
Chenyin