2269254_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2269254_en-US

2269254_en-US

install and updating the SDK for the S32K144 MCU

I have installed the S32 Design Studio to create project from the SDK example for the S32K144 MCU i am not able to found the SDK folder to configure the example project i have installed the SDK for the S32 K144 Device below i have share my problem regarding images please refer 

thank you in advance 

Re: install and updating the SDK for the S32K144 MCU

Hi

Please install the other two packages, then you will find the S32K1 RTD.

S32DS Extensions and Updates install S32K1 RTD300 QLP03.pngS32DS Extensions and Updates install S32K1 RTD300 QLP03.png

I remember that previously, I only needed to select one of them, and the S32K1 RTD-related dependency packages would be installed automatically.

Please note that during the Christmas holiday period, our support response times may be longer than usual. In some cases, your request might be addressed after the New Year. Thank you for your understanding.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

Tags (1)
No ratings
Version history
Last update:
‎12-30-2025 02:28 AM
Updated by: