Dera suport,
I generated the FSS FW 1.14.0 from Tresos
and executed make build from
C:\NXP\S32N_FSS_FW_R21-11_1.14.0\eclipse\plugins\Fss_Firmware_TS_T31D62M114I0R0\examples\EBT\Firmware_S32N79_FSS>
towards teh end of the process during linking I get below error
c:/nxp/s32ds.3.6.5/s32ds/build_tools/gcc_v11.4/gcc-11.4-arm32-eabi/bin/../lib/gcc/arm-none-eabi/11.4.0/../../../../arm-none-eabi/bin/real-ld.exe: out/Os_cfg_c.o:(.osrodata+0x7f0): undefined reference to `FuncTASK_DDR1_DATA_INIT_STATUS'
collect2.exe: error: ld returned 1 exit status
make: *** [Makefile:635: main.elf] Error 1
I rechecked the FSS FW delivery and found references to function
FuncTASK_DDR1_DATA_INIT_STATUS
but there is no implementation in the delivery.
Also FSS User Manual does not mention this function. Any hint on how to deal with the error ?
I used the FSS FW 1.14.0 out of the box - no adjustments no changes.
Best REgards,
Viktor
FuncTASK_DDR1_DATA_INIT_STATUS will be generated in Fss_Ddr_Cfg.c of Fss_Firmware when "Os Task Reference" node is enabled.
For Fss Firmware example of 1.14.0 release. We already enabled them with Os configuration together. So please re-check your Fss_Frimware.xdm configuration.