I need to use the A1006UK chip, have done the engineer contact me I need to use the A1006UK chip. Engineers who have done it have contacted me. Thank you very much, vx jesssaid
Hi @jesssiad.
The A5000/A30 and A1006 are not pin2pin compatible, but are AUTHENTICATORS, and customers can develop application code through the corresponding middleware.
A5000: https://www.nxp.com/webapp/Download?colCode=SE05x-PLUG-TRUST-MW &appType=license
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the " Mark Correct " button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
A5000 or A30 pin-to-pin?
Hi @jesssaid.
This part is already obsolete, if you are making a new product, the A5000 or A30 is recommended.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the " Mark Correct " button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
There are products using NXP A1006, have done the trouble to exchange, thank you!
How do you do that with an old product? Thank you.
Need a 4pin A30 as a replacement?