2266890_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2266890_en-US

2266890_en-US

Inquiry about Safety Peripheral Drivers (SPD) for FS32K144HAT0MMHT – Availability and Free Source

Hi team,

We are starting a new ISO 26262 (ASIL-B) project using the FS32K144HAT0MMHT MCU and want to understand how the Safety Peripheral Drivers (SPD) work.

Where can we download the SPD package, and do we need a specific package name like SW32K1-SPD-D in the NXP Software License & Support portal?

Is SPD free or included with standard RTD/SDK downloads, or does it require a separate license?

Are there any example or free sources available to study SPD drivers for early development?

Any guidance on locating SPD or related resources would be appreciated.

Thank you!

Re: Inquiry about Safety Peripheral Drivers (SPD) for FS32K144HAT0MMHT – Availability and Free Sourc

Hi @KAVINKUMAR7,

The S32K1 – Safety Peripheral Drivers (SPD) includes only the following driver:
Extended MCEM Driver for S32K1, Version 1.0.1

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K1-SPD-D&_gl=1*ao7djc*_ga*M....

The driver is included in the S32K1xx Standard Software package, which is available free of charge.
It is compatible with the S32K1/S32M24x Real-Time Drivers, ASR R21-11, Version 2.0.0 P04.
However, no functional example is provided for this driver.


Regards,

Daniel

Re: Inquiry about Safety Peripheral Drivers (SPD) for FS32K144HAT0MMHT – Availability and Free Sourc

Hi,

This SPD supports production. Could you please confirm whether it is suitable for use in a production environment?

Re: Inquiry about Safety Peripheral Drivers (SPD) for FS32K144HAT0MMHT – Availability and Free Sourc

Hi @KAVINKUMAR7,

Yes, it does. Please refer to the release notes.

This version is at RTM (Ready to Manufacture) level.

danielmartynek_0-1766921833541.pngdanielmartynek_0-1766921833541.png

Regards,

Daniel


Re: Inquiry about Safety Peripheral Drivers (SPD) for FS32K144HAT0MMHT – Availability and Free SourcHi,

Thank you for the response.

I have installed the latest S32 Design Studio IDE and used the RTM (Ready to Manufacture) RTD SDK as mentioned in the release notes. The CAN sample project was generated directly using the provided SDK and configuration tools.

However, even with this setup, I am still facing the following build error:

fatal error: Port_Ci_Port_Ip_Types.h: No such file or directory

Error occurs at: 

board/Port_Ci_Port_Ip_Cfg.c:56
#include "Port_Ci_Port_Ip_Types.h"
Re: Inquiry about Safety Peripheral Drivers (SPD) for FS32K144HAT0MMHT – Availability and Free Sourc

Hi @KAVINKUMAR7,

It appears that this is a compatibility issue.

In the correct S32DS IDE version, only the compatible RTD and the SPD specified in the SPD release notes should be installed. No additional RTD versions should be present. If you require multiple RTD versions, we recommend installing separate IDE instances.

Since your follow-up question is no longer related to the SPD, please create a new thread if you need further assistance.


Regards,

Daniel

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎01-03-2026 02:24 AM
更新者: