2264557_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2264557_en-US

2264557_en-US

S32K396 ADC

Our processor is S32K396. When using ADC, the following error occurred:
I have a total of 5 ADCs. Two of them use the channels 1 and 3 of the AD5 controller respectively. Occasionally, there will be abnormal data collection from channel 1. At this time, by measuring with a multimeter, there is voltage on the pins, but no values can be obtained. When channel 3 is shielded, channel 1 works normally.
The remaining 3 channels of ADC are each using a separate AD controller, and all are functioning properly.
The attachment contains the configuration of my AD5 components and the ADC acquisition code. Please take a look and let me know if there are any issues.
Thank you!

我们处理器为S32K396,使用ADC时出现如下错误:

我共有5路ADC,其中有两路分别用了AD5控制器的通道1和通道3;此时会偶发性出现通道1采集异常,此时通过万用表测量管脚上存在电压,但是采集不到值。当把通道3屏蔽掉之后,通道1工作正常。

剩余3路ADC分别单独使用一个AD控制器,均工作正常。

附件是我的AD5组件配置及ADC采集代码,麻烦看下什么问题。

谢谢!

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎12-19-2025 02:30 AM
更新者: