2256041_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2256041_en-US

2256041_en-US

S32K5 RTD problem using Ethernet driver

Hello,

Question from Schaeffter on S32K5 0.4.5 RTD Ethernet driver

The first issue that we see is the following :                      

nxp52415_0-1764926552510.png


                Out of all registers only PCI_HDR_TYPE0 is initialized , the other ones are not :
               

nxp52415_1-1764926552521.png




                The first hard fault comes because OSR register is accessed and because it is not initialized we have the fault :
               

nxp52415_2-1764926552578.png


Priority: CRITICALRTDRe: S32K5 RTD problem using Ethernet driver

Hi @nxp52415 ,

I'm using the package SW32K5_RTD_R23-11_0.8.0_CD03. In this package, the example Eth_netcv4_InternalLoopback_S32K566_M7 was attached, so you can refer to it.

In your image, you are still in initialization of Port switch, after this command, Port switch registers will be activated to access.

Nhi_Nguyen_0-1765186070152.png

Nhi_Nguyen_1-1765186106970.png

But this doesn't active NETC controller.

Nhi_Nguyen_2-1765186172178.png

NETC will be activated in the function Eth_43_NETCV4_Init(), like this:

Nhi_Nguyen_3-1765186286257.png

Please migrate to the latest package, the package SW32K5_RTD_R23-11_0.8.0_CD03 is even code drop qualification, So 0.4.5 is too old.

Best regards,

Nhi


タグ(1)
評価なし
バージョン履歴
最終更新日:
‎12-09-2025 04:26 AM
更新者: