2253000_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2253000_en-US

2253000_en-US

Zephyr:Booting DSP from MCU in Zephyr

Hello, I am currently working on a project using the RT595 with the Zephyr RTOS, and I want to know how to start the DSP from the MCU. According to section 4.7 of the official documentation (IMXRT595-EVK-UG), by setting DSP_IMAGE_COPY_TO_RAM=1in the IDE, it is possible to achieve "program once, and the ARM core automatically wakes up the DSP". Now that the project has fully transitioned to the Zephyr build system, I would like to know the specific steps to launch the DSP application and how it should be configured. Thank you for your help.

Evaluation BoardRe: Zephyr:Booting DSP from MCU in Zephyr

@jingqi 

General Steps:

To launch the DSP from the MCU in a Zephyr project, you should first build the DSP binary with Xtensa Xplorer, then integrate that binary into your Zephyr build via CMake, and finally call the BOARD_DSP_Init() function from your application to handle the startup sequence.


You need to complete the functionality using the official documentation (MCUXpresso + EVK) and you need to have the ability to develop Zephry before you can complete the migration.


Refernce:

1. Build the DSP Firmware: Getting Started with Xplorer for EVK-
MIMXRT595 Typically, you will get two output files, such as dsp_text_release.bin and dsp_data_release.bin. These are the firmware images that the Cortex-M33 core will load into the DSP's RAM

2. Integrate the DSP Binary into the Zephyr Build: 
the Zephyr build system requires you to explicitly include these binary files in your Cortex-M33 application. You can do this by modifying the CMakeLists.txt file for your Zephyr application. You may need to use Zephyr's build system features (like zephyr_file_copy or by defining them as a binary blob) to place the files in a known location in the final firmware image.

3. The MCUXpresso SDK for the i.MX RT595 provides a driver ( fsl_dsp.c / .h ) to manage the DSP lifecycle. Zephyr for NXP devices includes this SDK, so you can call these functions directly from your Zephyr application code. Details can be found from '3.3 DSP Core Initialization' of Getting Started with Xplorer for EVK-
MIMXRT595

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎12-03-2025 02:26 AM
更新者: