Hello.
I tried to use EBtresos in AUTOSAR but it failed to activate.
B25C-AEBB-4319-BAB1 (valid until 06/30/2026)
ERROR: flxActAppActivationSend (50040,41147,10248)
The number specified exceeds the maximum number allowed (0).
Connection to FlexNet Operations Server failed.
So I need another activation code to use EBtresos.
Hello,
I am trying to use EBtresos in AUTOSAR, but activation failed.
B25C-AEBB-4319-BAB1 (valid until 06/30/2026)
ERROR: flxActAppActivationSend (50040,41147,10248) The specified number exceeds the maximum allowed number (0).
Connection to FlexNet Operations Server failed.
Therefore, I need another activation code to use EBtresos.
The reason is that there are none free licenses with this activation code. You will find always latest code in your NXP SW account under tresos download.
If the code is depleted it usually takes few days, until EB provide us with the new one.
Best regards,
Peter
Hello,
If you require permanent license, I suggest you to get in touch with EB.
Licenses we are getting are evaluation and will always expire after trial period.
There is no automatic notification for such. You will find the new license on the SW account once available:
Best regards,
Peter
Have you solved your problem??I have the same question?