2252687_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2252687_en-US

2252687_en-US

SPI Serial Boot Issues on MIMXRT595-EVK

I am working with the MIMXRT595-EVK​ evaluation board and am attempting to use the ROM bootloader for serial download via the SPI interface. My goal is to communicate with the bootloader and download an application image through SPI, similar to how it is commonly done via UART.

Here is my current situation:

First, I successfully verified that the ROM bootloader is functional by performing a serial download via UART(J26)

 Then I am now trying to use the SPI interface on header J36​ (pins 1-CS, 3-MOSI, 5-MISO, 7-SCK) for the serial download process.When I probe the signals with an oscilloscope, the MISO line (J36, pin 5) shows an incorrect and jittery waveform​ during the ISP communication attempt. 

Questions and Points of Confusion:

I suspect that the SPI signals from the J36 header may not be properly routed to the MCU pins used by the ROM boot.

​ I have noticed references to a J10​ header in the board documentation, but it is not physically present on my EVK.

In summary, since UART-based serial download works flawlessly, the issue appears to be specific to the SPI hardware path. My primary questions concern the correct jumper settings for J36​ to enable the SPI serial downloader and the relevance of the documented but missing J10​ header.

wx1_2-1764643640876.png



wx1_1-1764643389452.png

i.MX-RT500 

Boot ROM|Booting | FlashSecurity(Edgelock | secure boot | OTP)Re: SPI Serial Boot Issues on MIMXRT595-EVKThanks for the reply, I tried to replace it with another board and it works later
Tags (1)
No ratings
Version history
Last update:
‎12-09-2025 03:40 AM
Updated by: