2250433_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2250433_en-US

2250433_en-US

PEmicro Connection Assistant Issue on S32K3X4EVB-T172

I'm unable to connect to S32K3X4EVB-T172, despite following the Quick Start Guide: https://www.nxp.com/document/guide/quick-start-guide-for-s32k3x4evb-board:GS-S32K3X4EVB-Q172


Board and LEDs:

zaighamkhawaja_4-1764249676294.pngzaighamkhawaja_4-1764249676294.png


When attempting debugging, the PEmicro Connection Assistant shows up.

zaighamkhawaja_0-1764249542881.pngzaighamkhawaja_0-1764249542881.png


Device Drivers:

zaighamkhawaja_1-1764249590231.pngzaighamkhawaja_1-1764249590231.png

Debug Settings:

zaighamkhawaja_2-1764249639854.pngzaighamkhawaja_2-1764249639854.png

zaighamkhawaja_3-1764249653892.pngzaighamkhawaja_3-1764249653892.png

Already tried changing data cables, changing computers, reinstalling S32DS, reinstalling Drivers, trying P&E Micro Utilities.

Windows 11, tried on S32DS 3.6.4 & 3.6.1

S32K3X4EVB-T172 S32DS-S32PLATFORM OPENSDA 

Re: PEmicro Connection Assistant Issue on S32K3X4EVB-T172

Is this the first time trying to connect to the EVB? Was there any project uploaded to it before?

The board has is brand new and it seems to have some factory-installed programme i.e. the USER_LED_0 color changes by pressing SW5 and SW6

I can see from the picture both LEDs RESET_K3 and RST_OSDA are on. Is RESET_K3 always on when powering the board?
Are you able to measure it? Usually when the reset LED is on, the line is being pulled for a really short period of time periodically, keeping the MCU on reset.

RESET_K3 and RST_OSDA are OFF initially when I connect the board following the power-up procedure. When attempting to debug, the RST_OSDA (and sometimes RST_K3) LEDs turn ON while simultaneously getting the PEmicro Connection Assistant popup.

Also, if I press the SW4 and then retrying debugging, I get this different popup:

zaighamkhawaja_0-1764732467636.pngzaighamkhawaja_0-1764732467636.png

Also, measure the voltage sources, if these do not provide the expected value this means that the MCU could be damaged.

I've already tried with 2 different adapters: 12V-4A and 12V-5A, getting same results. The adapter voltage output is stable. 

- If you mean the S32K3 MCU getting damaged: The default application (LED color changing) is still working on the board.
- If you mean the NXP K26 getting damaged: I'm still able to upgrade the firmware using the "Multilink Firmware Config Utility" to usbmlacpembeddedens.1098

If you have any external debuggers available (PEmicro, JLink, Latuerbach, etc.), you can try using them instead to see if any connection is possible.

I'll get a JLink next week, along with a new EVB. This time it will be a S32K344MINI EVB.

If there's anything additionally required to identify the rootcause, let me know.

Zaigham

Re: PEmicro Connection Assistant Issue on S32K3X4EVB-T172

Hi @zaighamkhawaja,

Thank you for sharing your installation details. It seems both S32K3x Dev. package and PEmicro plugins are correctly installed. Is this the first time trying to connect to the EVB? Was there any project uploaded to it before? 

I can see from the picture both LEDs RESET_K3 and RST_OSDA are on. Is RESET_K3 always on when powering the board? Are you able to measure it? Usually when the reset LED is on, the line is being pulled for a really short period of time periodically, keeping the MCU on reset.

Also, measure the voltage sources, if these do not provide the expected value this means that the MCU could be damaged.

If you have any external debuggers available (PEmicro, JLink, Latuerbach, etc.), you can try using them instead to see if any connection is possible.

Best regards,
Julián


Re: PEmicro Connection Assistant Issue on S32K3X4EVB-T172

Sure, here it is:

zaighamkhawaja_0-1764623301449.pngzaighamkhawaja_0-1764623301449.png


zaighamkhawaja_1-1764623365030.pngzaighamkhawaja_1-1764623365030.png




  C/C++ Common GDB Support	11.4.0.202309142347	org.eclipse.cdt.gdb.feature.group	Eclipse CDT
  C/C++ Development Platform	11.4.0.202311271618	org.eclipse.cdt.platform.feature.group	Eclipse CDT
  C/C++ Development Tooling Native Utilities	11.4.0.202311271618	org.eclipse.cdt.native.feature.group	Eclipse CDT
  C/C++ Development Tools	11.4.0.202311271618	org.eclipse.cdt.feature.group	Eclipse CDT
  C/C++ DSF GDB Debugger Integration	11.4.0.202309151124	org.eclipse.cdt.gnu.dsf.feature.group	Eclipse CDT
  C/C++ GCC Cross Compiler Support	11.4.0.202309151124	org.eclipse.cdt.build.crossgcc.feature.group	Eclipse CDT
  C/C++ GDB Hardware Debugging	11.4.0.202309151124	org.eclipse.cdt.debug.gdbjtag.feature.group	Eclipse CDT
  C/C++ GNU Toolchain Build Support	11.4.0.202311121705	org.eclipse.cdt.gnu.build.feature.group	Eclipse CDT
  C/C++ GNU Toolchain Debug Support	11.4.0.202309151124	org.eclipse.cdt.gnu.debug.feature.group	Eclipse CDT
  C/C++ Memory View Enhancements	11.4.0.202309151124	org.eclipse.cdt.debug.ui.memory.feature.group	Eclipse CDT
  C/C++ Remote Launch	11.4.0.202309142347	org.eclipse.cdt.launch.remote.feature.group	Eclipse CDT
  Core Server Feature	1.15.200.v20231110-1900	org.eclipse.equinox.server.core.feature.group	Eclipse Equinox Project
  e(fx)clipse - IDE - Basic	3.9.0.202210170554	org.eclipse.fx.ide.basic.feature.feature.group	Eclipse.org
  ECF Apache Httpclient 5 FileTransfer Provider	1.1.702.v20231114-1017	org.eclipse.ecf.filetransfer.httpclient5.feature.feature.group	Eclipse.org - ECF
  ECF Core Feature	1.6.2.v20231021-2127	org.eclipse.ecf.core.feature.feature.group	Eclipse.org - ECF
  ECF Filetransfer Feature	3.14.1900.v20230715-1945	org.eclipse.ecf.filetransfer.feature.feature.group	Eclipse.org - ECF
  ECF Filetransfer SSL Feature	1.1.402.v20231021-2127	org.eclipse.ecf.filetransfer.ssl.feature.feature.group	Eclipse.org - ECF
  Eclipse Help System	2.3.1600.v20231201-0110	org.eclipse.help.feature.group	Eclipse.org
  Eclipse Platform	4.30.0.v20231201-0512	org.eclipse.platform.feature.group	Eclipse.org
  Eclipse RCP	4.30.0.v20231201-0512	org.eclipse.rcp.feature.group	Eclipse.org
  Eclipse XML Editors and Tools	3.31.0.v202308200343	org.eclipse.wst.xml_ui.feature.feature.group	Eclipse Web Tools Platform
  Embedded C/C++ J-Link Debugging	6.4.0.202307251916	org.eclipse.embedcdt.debug.gdbjtag.jlink.feature.group	Eclipse Embedded CDT
  EMF - Eclipse Modeling Framework Core Runtime	2.36.0.v20231002-1156	org.eclipse.emf.ecore.feature.group	Eclipse Modeling Project
  EMF Common	2.30.0.v20230916-0637	org.eclipse.emf.common.feature.group	Eclipse Modeling Project
  EMF Ecore Edit	2.16.0.v20230211-1150	org.eclipse.emf.ecore.edit.feature.group	Eclipse Modeling Project
  Equinox p2, headless functionalities	1.7.0.v20231112-1314	org.eclipse.equinox.p2.core.feature.feature.group	Eclipse.org - Equinox
  Equinox p2, minimal support for RCP applications	1.4.2200.v20231112-1314	org.eclipse.equinox.p2.rcp.feature.feature.group	Eclipse.org - Equinox
  GDB Client for Arm Embedded Processors 15.1 Build 1703	1.0.0.202511261537	com.nxp.s32ds.brc.gdb.tools.feature.feature.group	NXP
  GEF Classic Draw2d	3.18.0.202311222042	org.eclipse.draw2d.feature.group	Eclipse GEF
  GEF Classic GEF (MVC)	3.18.0.202311222042	org.eclipse.gef.feature.group	Eclipse GEF
  GEF Classic Zest	3.18.0.202311222042	org.eclipse.zest.feature.group	Eclipse GEF
  Git integration for Eclipse	6.8.0.202311291450-r	org.eclipse.egit.feature.group	Eclipse EGit
  GNU ARM PEMicro Interface Debugging Support	6.0.9.202509241532	com.pemicro.debug.gdbjtag.pne.feature.feature.group	P&E Microcomputer Systems Inc.
  Memory Analyzer	1.15.0.202311170814	org.eclipse.mat.feature.feature.group	Eclipse Memory Analyzer
  Nebula Grid Widget	1.1.0.202303072132	org.eclipse.nebula.widgets.grid.feature.feature.group	Eclipse Nebula
  net.sourceforge.ehep	1.1.0	net.sourceforge.ehep.feature.group	Randallco and EHEP Team
  NXP GCC for Arm Embedded Processors 10.2 Build 1728	1.0.0.202508270740	com.nxp.s32ds.brc.arm.tools.gcc102.feature.feature.group	NXP
  NXP GCC for Arm Embedded Processors 11.4 Build 1763	1.0.0.202508271006	com.nxp.s32ds.brc.arm.tools.gcc114.feature.feature.group	NXP
  PEmicro ARM Device Expansion Plugin	6.0.9.202509241532	com.pemicro.debug.gdbjtag.pne.expansion.feature.feature.group	P&E Microcomputer Systems Inc.
  Remote Services	11.4.0.202309142347	org.eclipse.remote.feature.group	Eclipse CDT
  Remote System Explorer End-User Runtime	4.5.500.202305261020	org.eclipse.rse.feature.group	Eclipse TM Project
  RTD S32K3XX	6.0.0.202506161748	com.nxp.RTD.S32K3XX.feature.feature.group	NXP Semiconductors, Inc.
  RTD S32K3XX	6.0.0.202506161748	com.nxp.RTD.S32K3XX.root.feature.feature.group	NXP Semiconductors, Inc.
  S32 Debugger Core	3.6.5.202511272018	com.nxp.s32ds.brc.debugger.core.feature.feature.group	NXP
  S32 Design Studio CLE S32CT	1.8.9.202511261304	com.nxp.s32ds.cle.uct.feature.feature.group	NXP
  S32 Design Studio for S32 Platform	3.6.5.202511272206	com.nxp.s32ds.platform.ide.feature.feature.group	NXP
  S32 Design Studio for S32 Platform Tools	3.6.5.202511272206	com.nxp.s32ds.platform.ide.tools.feature.feature.group	NXP
  S32DS Product	3.6.4.202509291703	com.nxp.s32ds.platform.ide.product	NXP
  S32G development package	3.6.4.202509291633	com.nxp.s32ds.s32g2.dev.feature.feature.group	NXP
  S32K1xx development package	3.6.5.202511272256	com.nxp.s32ds.s32k1.dev.feature.feature.group	NXP
  S32K3 FreeMASTER Serial Communication Driver	1.4.2.202412201001	com.nxp.s32ds.s32k3.sdk.freemaster.feature.feature.group	NXP
  S32K3xx development package	3.6.4.202509291639	com.nxp.s32ds.s32k3.dev.feature.feature.group	NXP
  S32M2xx development package	3.6.4.202509291626	com.nxp.s32ds.s32m2.dev.feature.feature.group	NXP
  S32N5 development package	3.6.4.202509291626	com.nxp.s32ds.s32n.dev.feature.feature.group	NXP
  S32R41 development package	3.6.4.202509291624	com.nxp.s32ds.s32r41.dev.feature.feature.group	NXP
  S32R45 development package	3.6.4.202509291624	com.nxp.s32ds.s32r45.dev.feature.feature.group	NXP
  S32R47 development package	3.6.4.202509291625	com.nxp.s32ds.s32r47.dev.feature.feature.group	NXP
  S32Z2/E2 development package	3.6.4.202509291631	com.nxp.s32ds.s32esz.dev.feature.feature.group	NXP
  SAF85xx development package	3.6.4.202509291625	com.nxp.s32ds.saf85.dev.feature.feature.group	NXP
  SAF86xx development package	3.6.4.202509291626	com.nxp.s32ds.saf86.dev.feature.feature.group	NXP
  SECRDR S32K1	3.0.0.202508081221	com.nxp.SECRDR.S32K1.feature.feature.group	NXP Semiconductors, Inc.
  Terminal (Console) View	11.4.0.202311142324	org.eclipse.tm.terminal.view.feature.feature.group	Eclipse CDT
  TM Terminal	11.4.0.202309142347	org.eclipse.tm.terminal.feature.feature.group	Eclipse CDT
  TM Terminal Control	11.4.0.202311142253	org.eclipse.tm.terminal.control.feature.feature.group	Eclipse CDT
  TM Terminal Local Connector Extensions	11.4.0.202309142347	org.eclipse.tm.terminal.connector.local.feature.feature.group	Eclipse CDT
  TM Terminal SSH Connector Extensions	11.4.0.202309142347	org.eclipse.tm.terminal.connector.ssh.feature.feature.group	Eclipse CDT
  Xtend Library	2.33.0.v20231121-0955	org.eclipse.xtend.lib.feature.group	Eclipse Xtext



 

Re: PEmicro Connection Assistant Issue on S32K3X4EVB-T172

Thank you for your interest in our products and for contributing to our community.

Let's take a step back first, please.

Please an screenshot of your "Installation Details", which you can find in "Help" tab of the IDE.

Re: PEmicro Connection Assistant Issue on S32K3X4EVB-T172

Hi @zaighamkhawaja,

Thank you for the additional info.

Please update me if you can connect with the external debugger.  

Does this happen with a blank or an example project? As a last chance, have you tried to attach to the MCU instead of trying to debug/erase?

Julin_AragnM_0-1764966031025.pngJulin_AragnM_0-1764966031025.png

This leads me to believe either HSE is installed, or the debug port is locked and needs to be unsecured by password or challenge/response. PEmicro provides Python scripts to authenticate the debugger at the start of each session; however, the password is needed.

Last resource can be to swap MCU to confirm if debug interface is faulty, or the MCU is secured/disabled debug pins.

Best regards,
Julián

Re: PEmicro Connection Assistant Issue on S32K3X4EVB-T172- External JTAG debugger works.
- Empty or Sample projects also did not work.
- Attach to Running Target did not work.

I also purchased another board and that works with the onboard debugger, so nothing related to IDE or config settings.
タグ(1)
評価なし
バージョン履歴
最終更新日:
‎04-05-2026 02:26 AM
更新者: