2248341_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2248341_en-US

2248341_en-US

Is DDR ISSI LPDDR4 IS46LQ32K01S2A-046BLA1 compatible and supported with iMX8MPlus Processor?

Hi,

We are working with on a hardware with iMX8MPlus processor. We intend to use the ISSI LPDDR4 P/N IS46LQ32K01S2A-046BLA1 as the memory source.
 
We request a confirmation from NXP engineers that the ISSI IS46LQ32K01S2A-046BLA1 is fully compatible and validated for use with the NXP i.MX8MP processor.

Adding links to members:

@pradeep_t 

@GOWRIPRIYA_G 

Re: Is DDR ISSI LPDDR4 IS46LQ32K01S2A-046BLA1 compatible and supported with iMX8MPlus Processor?

Hi @naikabhishek,

Thank you for contacting NXP Support!


According to our memory compatibility guide, the part number that you want to use is compatible with iMX8MP.

We have validated the S46LQ32K01S2A-046BLA2 and IS43LQ32K01S2A-046BLI, according with the datasheet the part with ending A1 only changes the temperature range.


Best Regards,

Chavira

标记 (1)
无评分
版本历史
最后更新:
‎11-26-2025 08:32 PM
更新人: