2201028_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2201028_en-US

2201028_en-US

Can i use MIMXRT1060-EVK default firmware for MIMXRT1060-EVKB

Hi, I have been looking through some tutorials when the board is stuck and I get the error: 0 available SWD Devices detected.

When I researched and reloaded the firmware for the board. In my pc I did not find the firmware for MIMXRT1060-EVKB but only the MIMXRT1060-EVK version

https://www.nxp.com/design/design-center/development-boards-and-designs/OPENSDA#MIMXRT1060-EVK

I wonder if it is possible to load that firmware.
Thanks everyone

Boot ROM|Booting | FlashRe: Can i use MIMXRT1060-EVK default firmware for MIMXRT1060-EVKB

Hi @cylasion,

It is possible to load the OpenSDA firmware from the MIMXRT1060-EVK onto the MIMXRT1060-EVKB.

OpenSDA firmware is loaded onto the FreeLink interface, and both the MIMXRT1060-EVK and MIMXRT1060-EVKB use an LPC432x device for this interface.

Best Regards,
Pablo

标记 (1)
无评分
版本历史
最后更新:
‎11-21-2025 04:53 AM
更新人: