2200071_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2200071_en-US

2200071_en-US

Greenish Tint in LCD Video Stream on i.MX RT1176

I’m working on live streaming a camera feed to an LCD display using the i.MX RT1176 controller.
The incoming H.264 video stream is decoded using FFmpeg into YUVJ420P pixel format with BT.709 colorspace.

On the RT1176 side, we use the PXP (Pixel Pipeline) for YUV-to-RGB conversion (CSC) before displaying the frames on the LCD. However, the displayed video has a noticeable greenish tint.

Since the PXP does not support the YUVJ420P pixel format directly, we configure the process surface buffer format as YUV420.
Also, when checking the CSC coefficient setup in the PXP driver (kPXP_Csc1YCbCr2RGB mode), the coefficient values appear to correspond to the BT.601 colorspace, although this isn’t clearly documented in the reference manual.

Could anyone confirm whether the default PXP CSC coefficients are indeed based on BT.601?
If so, could you please share the correct BT.709 coefficient values that can be programmed into the PXP CSC registers to achieve accurate color conversion?

Re: Greenish Tint in LCD Video Stream on i.MX RT1176

Hi @EdwinHz,

Thank you for your reply.

If possible, could you please provide the appropriate CSC1 coefficient values for BT.709 YUV-to-RGB conversion, compatible with the PXP’s internal YUV→RGB conversion formula?

Re: Greenish Tint in LCD Video Stream on i.MX RT1176

Hi @Anni,

You are correct. In order to properly convert for BT.709, you will need to manually change the CSC coefficients on the PXP_CSC1CoefficientSet() function.

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 05:26 PM
更新者: