2198802_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2198802_en-US

2198802_en-US

RW612 Matter Networking Example Demonstration

I want to give an example recently. One RW612ET module is the host, and five RW612ET modules are the slaves. The five slaves collect data and send it to the host. The host is connected to the upper computer.

The host controls one of the slaves at the appropriate time, that is, the slave sends data to the host, and the host can also send data to the slaves.

These six modules form one network. May I ask which example of the host using the SDK library and which example of the slave using the SDK library?

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 05:03 AM
更新者: