2198802_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2198802_en-US

2198802_en-US

RW612 Matter Networking Example Demonstration

I want to give an example recently. One RW612ET module is the host, and five RW612ET modules are the slaves. The five slaves collect data and send it to the host. The host is connected to the upper computer.

The host controls one of the slaves at the appropriate time, that is, the slave sends data to the host, and the host can also send data to the slaves.

These six modules form one network. May I ask which example of the host using the SDK library and which example of the slave using the SDK library?

Re: RW612 Matter Networking Example Demonstration

Hello!

According to Build Matter OTBR and Zigbee Bridge application, execute git clone https://github.com/nxp-appcodehub/dm-matter-zigbee-bridge-rw612.git

The examples, src, and third_party folders were not found in the dm-mater-zigbee-bridge-rw612 file, dm-matter-zigbee-bridge-rw612/examples/bridge-app/nxp。

Many files are missing, which makes it impossible to execute and compile them later.屏幕截图 2025-11-14 192328.png

Re: RW612 Matter Networking Example Demonstration

Hello! The nxp file was not found in dm-matter-zigbee-bridge-rw612/examples/bridge-app/

Re: RW612 Matter Networking Example Demonstration

Hello, @MrShen 

Can you please check this doc and let me know whether it can meet your requirement?

RW612 Matter OTBR and Zigbee Bridge User Guide


Best regards,

Christine.

回复: RW612 Matter Networking Example Demonstration

Should we use Matter or ZigBee? Did you not see ZigBee in the SDK import wizard?

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 05:03 AM
Updated by: