2198028_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2198028_en-US

2198028_en-US

After resetting, the s32k312 enters the HardFault_Handler abnormally

The chip used is s32k312, with the compiler version being S32DS3.5 and RTD3.0. During the production of uds-boot, some valid information is fixed in pflash at address 0x0043E000.

sensen_1_0-1762236756459.png

sensen_1_1-1762236817623.png


sensen_1_2-1762236843789.png


sensen_1_3-1762236858994.png

Program the bootloader into the chip, and then flash the app program via the host computer. After the first flash, you can use the internal watchdog timeout reset to ensure the program correctly enters the app. However, when the program is running in the app and another app flash operation is performed, the program enters the HardFault_Handler after resetting. Please help me check if there is a configuration issue, or if there is a standard configuration method. As long as the information is not fixed in p_flash, but instead written to 0x0043E000 through instructions later, the program can run normally.

Thank you very much for your support.


标记 (1)
无评分
版本历史
最后更新:
‎11-21-2025 05:04 AM
更新人: