2197997_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2197997_en-US

2197997_en-US

S32K342 HSE

Dear Sir:

We are a third-party programmer manufacturer.

The S32K342 programming flow has been completed.

After successfully programming the HSE file, repower on wait 5 seconds, and read 4039_C028h (bit 0) to confirm whether the HSE was successful.


However, I read out 0x000001C0 (bit 0 is 0, HSE Unsuccessful).

What other registers can I read to confirm whether the HSE was successful?

Thanks

Re: S32K342 HSE

Have you installed on virgin device or there were already some attempts to have installed FW before?
Could you provide following information?
SBAF version:
HSE FW version:
MU registers, FSR, GSR, etc:
HSE GPR3:
Is the "HSE_STATUS_INIT_OK" have been wait set to "1"?

In case AB SWAP, multiple resets may be required.

Recently I have discussed installation procedure over following thread:

https://community.nxp.com/t5/S32K/S32K3-HSE-Installation-differences-between-FULL-MEM-and-AB-SWAP/m-...

Hope it helps

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 05:28 PM
更新者: