Hi.
Create a new project in any folder.
After creating source files, etc., close the project.
When I start Presso and specify the project folder, it displays "No project selected" and all the source files are not displayed.
I have repeated this process many times. Is it okay to use anything other than the default?
Best regared.
Hello @tamotsu ,
Please refer to the screen recording attached. I conducted the following tests but failed to reproduce the issue you encountered. I am using MCUXPresso v25.6.
1.Create a new workspace.
2.Create a new project and add a source folder/source file to it.
3.Close MCUXpresso and reopen it.
Everything works normally.
You can also refer to the attached MCUXpresso user guide.
Hope it helps.
BR
Celeste
Hello Celecte.
This is the iMX7D M4.
At first, I wanted to create a unique directory, so I specified it as "Original_Dir.pnp".
In this case, when I restart MCUXpresso, I will get the error "No project select" after clicking IDE.
Strangely enough, when I set it to the default, "Default_Dir.pnp", it displayed correctly.
I don't know what the correct way to do it is actually.
Best regards.
Hello @tamotsu ,
Thanks for your post.
Could you tell me which MCU you are using? Additionally, to better reproduce and resolve your issue, could you help provide some screenshots or screen recordings?
BR
Celeste