2196132_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2196132_en-US

2196132_en-US

Load initial bootloader thought CAN interface?

Can the initial bootloader file be loaded through the CAN interface on a brand new MCU, thus eliminating the need for a JTAG connector?

Re: Load initial bootloader thought CAN interface?

Hello @klv222 

Please describe your question in more detail. Which chip are you referring to? Which bootloader file? 

Thank you.


BR

Alice


Re: Load initial bootloader thought CAN interface?

Yes, it is possible in some MCU families to load the initial bootloader through the CAN interface on a brand-new MCU, potentially eliminating the need for a JTAG connector, but this depends entirely on the MCU’s built-in features. Many modern microcontrollers ship from the factory with a ROM-resident bootloader that supports communication over interfaces such as CAN, UART, USB, or SPI. If CAN is supported in this factory bootloader, the MCU can be programmed directly via the CAN bus on first power-up, provided the correct boot mode pins or configuration are set. However, if the MCU does not include a CAN-capable ROM bootloader, JTAG or SWD is still required at least once to install an initial bootloader. Additionally, JTAG remains valuable for low-level debugging, recovery from misconfiguration, and unbricking devices, even if it is not required for normal production programming.   change healthcare

标记 (1)
无评分
版本历史
最后更新:
‎02-03-2026 03:22 AM
更新人: