Hi,
I am trying to figure out how to use a timer to improve low speed quadrature encoder measurements on i.MX RT1060. I can see in the reference manual (55.4.2 Prescaler for Slow or Fast Speed Measurement) that there should be some support for low speed measurements using a timer. However, I am having a hard time understanding how I can set this up? Are the some examples since this was posted?
If not could you provide a brief explanation of what I need to do? Does the ENC have its own timer or should I setup a separate timer? What are the steps for setting up such a timer?
Thanks!
Best regards,
Tor
Hi @Kan_Li ,
Thank you I have made a support case with the same title as this one.
Best regards,
Tor
Hello @RegulaTor ,
Yes, we have such kind of demo but it is just internal used, would you please raise a private case for it? Please kindly refer to https://www.nxp.com/video/tutorial-for-nxp-support-case-portal:NCP-VIDEO for details.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------