2193557_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2193557_en-US

2193557_en-US

i can't detect RT1062 with MCU-Link

Hello there, i am new to NXP products and i made a dev board using the RT1062 as its core componenet an i am having issues connecting to the it, i am using the MCU-link as a debbuger and i want to debug using SWD interface, i installed the drivers correctly and using LinkServer.exe in windows to try to probe the target. it detect the MCU link but not the RT1062 and i even tried with MCUXpresso IDE same result.

i based my design on the MIMXRT1060-EVKB-DESIGNFILE-RevB1 schematics and i routed the swd pins directly to a connector. i am messing something out ?? and doest boot configuration matter in this case ?

PS: all power rails are 3v3 besides USB which is 5V

i.MXRT 106xRe: i can't detect RT1062 with MCU-Link

Hi @yacineykr ,

Thanks for your updated information.

Please kindly check the FlexSPI NOR Device Configuration setting.

Especially you use the  second option pins. 

mayliu1_0-1761729173687.png

Best Regards

MayLiu

Re: i can't detect RT1062 with MCU-Link

Thanks for your reply,

i did that and the power sequencing is respected. 

i also tried to do a serial download by configuring the boot pins. i am using a NOR Flash from Winbond on FlexSPI second option pins (GPIO_AD_B1), the PC detects the MCU as an HID device using USB, but when i try to connect to boot ROM it tells me that the MCU has entered Flashloader but failed to configure external memory (i used MCU boot utility)

Re: i can't detect RT1062 with MCU-Link

Hi @yacineykr ,

Thank you so much for your interest in our products and for using our community.

1: I suggest you use an oscilloscope to check if the power-up sequence on the RT1060 board is correct. You can refer to MIMXRT105060HDUG for more detail information.

mayliu1_0-1761619618980.png

2: Please check whether you add PSWITCH RC delay.

mayliu1_1-1761619690540.png

3: Please compare the hardware design differences between your custom development board and the MIMXRT1060-EVKB development board.

Wish it helps you.
If you still have question about it, please kindly let me know.

Best Regards
MayLiu

标记 (1)
无评分
版本历史
最后更新:
‎11-21-2025 05:33 PM
更新人: