2193450_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2193450_en-US

2193450_en-US

Enabling USB Device Mode in U-Boot on RDB3 for eMMC Boot

Hi,

Recently, several customers have inquired about how to program the eMMC on the RDB3 development board directly via USB in U-Boot. These customers are designing custom boards based on RDB3 without using an SD card or Ethernet, and therefore need a method to flash the eMMC through USB during the setup stage.

By default, USB device mode is not enabled in U-Boot on RDB3. To achieve this functionality, it is necessary to modify the U-Boot and ATF (Arm Trusted Firmware) source code, as well as adjust the USB configuration to enable USB device support in U-Boot. In addition, the document provides guidance on testing the configuration, demonstrating how to use U-Boot commands to verify that the USB storage device is recognized, load the image from the USB into memory, and write it to the eMMC.

In this article, I will share my experience using BSP42 to implement and test this feature. I hope this guide will be helpful to others who are looking to enable USB device in uboot for eMMC programming on RDB3.

S32G
Tags (1)
No ratings
Version history
Last update:
‎11-20-2025 05:57 AM
Updated by: