2192532_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2192532_en-US

2192532_en-US

SJA1105P PHY MODE MAC to MAC connection issue

Hi,NXP

I'm currently encountering a connection issue with the SJA1105. I'm using S32K3 + SJA1105 + TJA1103.

At present, the data sent from the PHY to the SJA1105 can be forwarded to other ports, and the S32K3 can also receive the data from the SJA1105, and the data is correct.

However, after the S32K3 sends data to the SJA1105, the SJA1105 does not forward the data to other ports. I can see that there is a correct waveform received on the RXD pin of Port 0, but no waveforms are emitted from other ports.

What could be the possible problems? Do you have any suggestions?


Below are my hardware topology and script configurations.My script is modified using simplePQRS.py
wuxianlong_0-1761306087975.png
wuxianlong_2-1761306182326.png

Best Regards,
xianlong

Re: SJA1105P PHY MODE MAC to MAC connection issue
Thanks for your support. The RX_ER of my SJA1105 is not connected to ground
Re: SJA1105P PHY MODE MAC to MAC connection issue

Hi,

hard to suggest based on info provided. A topology and script modification looks correct.
Quick tip, be sure you have RX_ER grounded if not used on switch port 0.
To comment more please provide more info.
Could you share your full schematic, or part for S32K3 + SJA1105 + TJA1103 connection at least?
Could you share your sja1105_simple.py?

What kind of traffic do you have?

BR, Petr

Tags (1)
No ratings
Version history
Last update:
‎11-20-2025 10:17 AM
Updated by: