2191608_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2191608_en-US

2191608_en-US

S32N55: The configuration "EthSwtEnableSharedLearning" for NETC switch is not supported.

Hello Team,

RTD version: SW32N_RTD_R21-11_1.8.0_CD05

1. In EB Tresos, the configuration option EthSwtEnableSharedLearning is currently grayed out and not supported. It appears that the default value is set to true.
Hope this option can be made configurable in EB Tresos to support FID functionality.

2. Once EthSwtEnableSharedLearning becomes configurable and is set to false, the FID in the FDB table is able to configurated for independent vlan MAC learning. Currently, the FID in the FDB table is hardcoded as 0 in the driver.

Tangsheng_Zhou_0-1761227063215.png

Best regards,

Tangsheng.


Priority: MEDIUMRTDSource: Direct CustomerRe: S32N55: The configuration "EthSwtEnableSharedLearning" for NETC switch is not supporte

Hello @Nhi_Nguyen 

Thanks for your support.

Best regards,

Tangsheng.

Re: S32N55: The configuration "EthSwtEnableSharedLearning" for NETC switch is not supporte

Hi @Tangsheng_Zhou ,

SW team responded that they don't have plan to support this feature. If the customer want to have it please make the request.

Best regards,

Nhi


Re: S32N55: The configuration "EthSwtEnableSharedLearning" for NETC switch is not supporte

Hello @Nhi_Nguyen 

Thank you for your response.

Could you share if there are any plans to develop this feature?

If so, could you also provide the expected timeline?

Thanks!

Best regards,

Tangsheng.

Re: S32N55: The configuration "EthSwtEnableSharedLearning" for NETC switch is not supporte

Hi @Tangsheng_Zhou ,

All of drivers in this release are delivered with Pre-early quality. For features that you see as gray, they didn't support yet.

Best regards,

Nhi

标记 (1)
无评分
版本历史
最后更新:
‎11-20-2025 10:19 AM
更新人: