2189029_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2189029_en-US

2189029_en-US

Problems with lpc5606

Hello everyone, I recently switched from keil to MCUXpressoide, but encountered a bit of a problem, when I ported the program from keil to MCUXpressoide, compiled no problem, but after downloading it to let him run, it feels that he is running very slowly, because there is a three-digit digital tube on the board, the digital tube refreshes strangely, three 8- >three 0- >Specific numbers - >a certain one, please have any ideas?

LPC546xxRe: 使用lpc5606遇到的问题Thank you for your reply, so far I have solved this problem, I added osgi.nl=en_US in the config.ini file and the compiler changed to English language!Re: 使用lpc5606遇到的问题

Hello @xxxxyyyy


Please show the code.
Are you using GUI Guider?


BR

Alice.

Re: 使用lpc5606遇到的问题Sorry, it was my mistake, it was lpc54606, I've found the specific problem so far, it's the Chinese date displayed by the _date_ macro definition, do you know how to change it to English please.Re: 使用lpc5606遇到的问题

Hi @xxxxyyyy

1) LPC doesn't have LPC5606 series, are you using LPC5506?

2) It is recommended to check the clock configuration, after porting, the clock configuration maybe different, which affects the refresh speed.


BR

Alice.

Re: 使用lpc5606遇到的问题Hello, this is the case I'm currently showing an exception, I may not have described it clearly in my question, sorry!Re: 使用lpc5606遇到的问题

Hi @xxxxyyyy

May I ask if the binary is burned directly to the board and run off the IDE (disconnected from the debugger).

Are the actual operating results normal?


BR

Alice.

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 05:31 AM
更新者: