Hello:
I Create a new project, add port settings, and debug it. When debugging online, running the function (Port_Init(NULL_PTR);), the s32ds sortware will disconnected, as show:
after offline, the code can run normally and the port settings work properly. now The program cannot be debugged online。
Please take some time to answer, thank you!
Hi
It seems that you have modified the JTAG pins in 'UnTouchedPortPins' which caused debugging to break and the program cannot be downloaded normally. Please refer to the discussion in S32K344 RTD, PORT/DIO and Debugging
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------