The popup asks to update the project created under version 1.7.0 to 1.8.0, my current version is 1.10.0, first of all how do I update it to 1.8.0? and secondly does updating it to 1.8.0 make it possible to open it in the 1.10.0 version? A million thanks!
Hi @Suuu,
Due to changes on the GUI Guider toolchain, all projects created on v1.7.x must be upgraded to 1.8.x before updating them to any other subsequent version. Please first download v1.8.0, import your project to that version, and then follow the same process with 1.10.0. There is no need to go through 1.9.0.
Note that you will be prompted this message on each upgrade step:
Make sure to click OK to update the project, I recommend keeping the backup enabled just in case.
BR,
Edwin.
I imported the project created in 1.8.1 into 1.10.1, and after the backup was completed, it kept showing an upgrade failure message.