2186844_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2186844_en-US

2186844_en-US

RW610 WiFi Direct Implementation

Hi,

I'm looking to use the RW610 chipset for an upcoming project and was wondering whether its hardware can support Wi-Fi Direct. In addition, does anyone know where i can obtain application note or any documentation that explains the implementation and operation of Wi-Fi Direct for the RW610 chipset module.

Thank you so much in advance.


Re: RW610 WiFi Direct Implementation

Hello @Designer11, hope you are doing well and sorry for the late reply.

The Wi-Fi example "wpa_supplicant" within SDK version 25.09, is compatible with Wi-Fi Direct/P2P feature, however to enable the feature it is required to define the macro: CONFIG_WPA_SUPP_P2P inside the "wifi_config.h"  file.

For more information about WFD interface please refer to UM11442 on section 3.8.1.5.

Please let me know if this information is helpful.

Re: RW610 WiFi Direct Implementation

Hello @Designer11, hope you are doing well.

I will check this internally and I will inform you once I get a response from the internal team.

Thank you for your patience.

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 05:40 PM
Updated by: