Dear NXP support,
we are evaluating Jumbo Frames on LS1043A with a custom specific board, but when changing the MTU size in Linux the system shows:
Error: mtu greater than device maximum. During my research, I came across the following NXP Community thread:
https://community.nxp.com/t5/Layerscape/Why-is-LS1043-MTU-limited-to-2K-not-4K/m-p/847022
Which refers to FMAN Errata A-010022 and a patch to fix this behavior in the NXP LSDK Kernel.
But I did not find anything similar for Linux Mainline Kernel, are there any fixes NXP can provide to support Jumbo Frames ?
thank you in advance
Hello LFGP,
thank you for the reply, Since Layerscape CPUs are primarily intended for network equipment, we as manufacturer are very interested in using the Linux mainline kernel, as the platforms are supported for a very long time and we are not dependent on NXP for kernel updates. This is becoming increasingly important for us and our customers, especially in light of the Cyber Resilience Act.
best regards
Tim
Hello,
thanks for the reply, the mentioned option are only available in the NXP based Linux kernel, which uses CONFIG_FSL_SDK_DPAA
https://docs.nxp.com/bundle/UG10081_LLDP_L6.1.55_2.2.0/page/topics/jumbo_frames_support.html
In the Linux Mainline kernel CONFIG_FSL_DPPA_ETH is used which does not have the extended options in the kernel menuconfig
https://git.kernel.org/pub/scm/linux/kernel/git/stable/linux.git/tree/drivers/net/ethernet/freescale...
best regards
Tim