2184200_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2184200_en-US

2184200_en-US

Download the s32G274RDB2 program using the SJA1110 PE downloader on the switch

When the s32G274RDB2 was downloading the program using the SJA1110 PE downloader on the switch, the debug operation was normal. However, after repowering, when the switch was set to start from flash, the program would not be updated to the latest downloaded version. I want to know where the problem lies with my PE debug Settings?  Moreover, a month ago, I was able to download it normally, and when I repowered it, I could update it to the latest program normally. 

sdx111_0-1760154232482.pngsdx111_1-1760154262744.png

 

sdx111_3-1760154311544.pngsdx111_4-1760154332323.pngsdx111_5-1760154345607.png


Re: Download the s32G274RDB2 program using the SJA1110 PE downloader on the switch

Hello, @sdx111 

Thanks for your reply.

Sorry that I have not reproduced the issue from my side, by checking the logs shared, I do not see the log for VM and other commands, and I mentioned that seems you are still working with S32DS3.4, but combining with the SJA1110 SDK 1.0.2?

Since SJA1110 SDK 1.0.2 was released and tested on S32DS3.5, would you mind retesting it on S32DS3.5 for a trial?


BR

Chenyin

Re: Download the s32G274RDB2 program using the SJA1110 PE downloader on the switch

1、The dial-up operation should be carried out according to the following figure.

sdx111_0-1760182236451.pngsdx111_1-1760182250746.png

2、Print as shown in the following picture.

sdx111_2-1760182317028.pngsdx111_3-1760182336545.png



Re: Download the s32G274RDB2 program using the SJA1110 PE downloader on the switch

Hello, @sdx111 

Thanks for your post.

1. What is the switch setting when you flash the spi of SJA1110 and after repowering?

2. When flashed the binary, have you checked in the console with command VM? what are the prints?


BR

Chenyin

标记 (1)
无评分
版本历史
最后更新:
‎11-21-2025 11:26 PM
更新人: