Hi,NXP
I see that NXP's S32DS has now been updated to version 3.6.4. I previously installed version 3.6.2.
If I need to update the version, I have to install an additional IDE, reinstall RTD, recreate the workspace, and so on.
Why doesn't version 3.6.x continue from version 3.5.x and share one IDE? Instead, each minor version is made into a separate IDE.
What considerations are these based on? At present, I mainly use S32 series MCUs. What usage suggestions do you have?
Best Regards,
xianlong
Hi @wuxianlong
You can actually install S32DS v3.6.x updates in the same instance; Please refer to the installation guide that comes with v3.6.4:
I think this is rather buried under documentation, but a new installation is not needed:
Best regards,
Julián