2180047_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2180047_en-US

2180047_en-US

NXP Zephyr display portability demo

This simple demo shows the portability of Zephyr with LVGL by running the same application on different hardware platforms.  Leveraging Zephyr's Hardware Abstraction Layer (HAL), applications can be written without hardware dependencies in the source code.  And without changing source, the same app can be built for different hardware.

The demo steps use the following hardware and tools, but can easily run on other hardware with displays using the same general steps:

The attached presentation gives a brief overview of Zephyr and the HAL portability.  This video shows all the steps to build the example, prepare the hardware, and program the boards.


Return to Zephyr Knowledge Hub

标记 (1)
无评分
版本历史
最后更新:
‎11-19-2025 04:35 PM
更新人: