2179310_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2179310_en-US

2179310_en-US

S32K3xx Clock tool CMU

Hi team,

What is the purpose of these two options in the S32K3xx RTD Clock tool?

danielmartynek_0-1759404814580.png

If set, the configuration tool does not generate the notification in the generated code.

And, if used with the MCAL MCU driver (where the CMU is enabled), the CMU must be disabled in the Clock tool:

danielmartynek_1-1759404950883.png


Thank you,

BR, Daniel


RTDRe: S32K3xx Clock tool CMU

Hi @danielmartynek ,

This is also for RTM600.

The problem for your project is as notification displayed:

Nhi_Nguyen_0-1759828913005.png

Please make sure that CmuNotification is configured same configuration in all ClockConfig.

Nhi_Nguyen_1-1759829009843.png

Driver doesn't support multiple variants for this feature.

Best regards,

Nhi


Re: S32K3xx Clock tool CMU

Hi @Nhi_Nguyen,

I understand that.

The problem is in my RTD 6.0.0 IP test project, the notification function is not generated.

What RTD have you tested?


Regards,

Daniel


Re: S32K3xx Clock tool CMU

Hi @danielmartynek ,

If you enabled CMU in Clock tool only, you will have:

Nhi_Nguyen_0-1759477631825.png

This feature is exist in Mcu with difference implementation, so you just can enable one of them.

Nhi_Nguyen_1-1759478075555.png

Best regards,

Nhi


タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-20-2025 11:42 AM
更新者: