Hello,
i've some evk 1180, i've few problem with some pc to connect the target, in some pc (2) there is no way to connect evk for debugging, it finds MCU Link, but "0 available swd devices detected with MCUxpresso IDE" happen..
the same boards works to other pc.
the Version used is 25.x
pls help me to fix this problem on this pc ( we have also tried to use virtual machine on this pc but the problem is the same, also unistall and re-install all packages)
Thanks!
Hi @William_Weg
thank you for your update!
I was able to update FW on my side
I placed a jumper on JP3 and power cycled the whole EVK.
I am using this schematic revison:
What is the schematic revision that you are using? Does update also fails with CMSIS DAP?
Thank you,
Diego
Link flash with GUI is correctly connected
Hi Diego,
I'm sorry but in any case doesn't work.
jp3 is close for isp mode
Thank you for your update and report! ( @William_Weg please use similar path for finding the JLink FW on Linkserver 25.9 : C:\nxp\LinkServer_25.9.134\MCU-LINK_installer\scripts )
After first log in, I could install the version 25.9, So unfortunatelly I could not replicate the issue! but, I suggest to install Linkserver package directly from this page https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools...
Please let me know your results, guys
Diego
Hi @William_Weg
Please refer to the below image!
Diego
FYI we are trying to install 25.9 but on all pc we have this issue after first login ask:
[info] Downloading file https://www.nxp.com/lgfiles/updates/mcuxpresso/JLink_Windows_V872_x86_64.exe using axios
[info] Installing SEGGER J-Link (8.72)...
[info] Executing and elevating command "C:\Users\colombos\AppData\Local\Programs\MCUXpressoInstaller\.cache\JLink_Windows_V872_x86_64.exe -Silent=1 -InstUSBDriver=1"
[info] Checking hash for file C:\Users\colombos\AppData\Local\Programs\MCUXpressoInstaller\.cache\debug_common-25.09.tar...
[info] Downloading Additional NXP debugger support from https://www.nxp.com/lgfiles/updates/mcuxpresso/debug_common-25.09.tar
[info] Downloading file https://www.nxp.com/lgfiles/updates/mcuxpresso/debug_common-25.09.tar using axios
[info] Installing Additional NXP debugger support (25.09)...
[info] Extracting debug_common-25.09.tar to C:\Users\colombos\.mcuxpressotools/debug_common-25.09
[info] Checking hash for file C:\Users\colombos\AppData\Local\Programs\MCUXpressoInstaller\.cache\LinkServer_25.9.134.exe...
[info] Downloading LinkServer from https://www.nxp.com/lgfiles/updates/mcuxpresso/LinkServer_25.9.134.exe
[info] Downloading file https://www.nxp.com/lgfiles/updates/mcuxpresso/LinkServer_25.9.134.exe using axios
[info] Installing LinkServer (25.9)...
[info] Executing and elevating command "C:\Users\colombos\AppData\Local\Programs\MCUXpressoInstaller\.cache\LinkServer_25.9.134.exe /VERYSILENT /SUPPRESSMSGBOXES"
[info] Checking hash for file C:\Users\colombos\AppData\Local\Programs\MCUXpressoInstaller\.cache\MCUXpresso_Config_Tools_v25.09_x64.exe...
[error] Error occurred while installing MCUXpresso Configuration Tools: self signed certificate in certificate chain. Skipping...
*** Installation error ***
Hi, I a Simone's collegue I have this problem in my pc and I Installed last version of LinkServer, on-board LPC55 but nothing changes. I want understand where i can find il JlinkFW mentioned in "try testing with JLink FW", thaks
Thanks Diego,
all pc with this problem is winodws 11 pro 24H2 build 26100.6584 the same as mine (that works). we have just tried to download the latest link server, the Lpc55 onboard is the latest version. as i said i can use (with another collegue) the boards with no problem, it runs correctly but the other two collegue there is no way to works!
what i can do?
FYI i'm working on a 24.x skd version (because i can't update for TSN support) and works correctly also with this version.
Please try to install the latest version of the Linkserver on that machine. Lets see if installing the drivers makes a difference. What is your OS? Do all the machines have the same OS and version?
Also, try to update the on-board LPC55 to run the latest version of CMSIS DAP. If this does not make any change at all, try testing with JLink FW. Let me know if you need more steps for this!
Diego