Hi,
Is the software source for this application note available? I can't seem to find it in the SDK example prowser within mcuxpresso.
Thanks
Hello @tristand,
The evkbmimxrt1060_lwip_dhcp_usb_bm example, which is used as the base in the application note, can be found in the SDK (version 2.16) examples, as shown in the following figure:
Where you can download the SDK through SDK builder.
At the same time, you can download the SDK inside MCUxpresso IDE clicking the next button:
Inside to the window called "Download and install SDK" you can search the evkmimxrt1060 in the filter, where it will be showing the available SDK, as shown in the next image:
BR
Habib