Content in imx93 timer is not executed.bsp:real-time-edge-3.1.0.xml
The /etc/net-debug.sh file is executed regularly in /etc/crontab, but now this script doesn't run. What is the reason?

Re: Content in imx93 timer is not executed.I can use the timing function by putting the crontab file into the /etc/cron.d/ file.Re: Content in imx93 timer is not executed.Hello,
Common Reasons for a Failed Cron Job
- Permissions: The script lacks execute permissions. You need to make the script executable using
chmod +x /path/to/your/script.sh.
- Path Environment Variable: Cron runs scripts in a minimal environment with a restricted
PATH. Commands within the script may not be found.
- Missing or Incorrect Paths:
- The crontab entry itself might use relative paths, which is problematic for cron.
- The script might not specify the full path to commands it calls (e.g., instead of
ls, use /bin/ls).
- Crontab Syntax Errors:
- There must be a newline character after the last command in the crontab file.
- The
user field is missing in the /etc/crontab file, which requires a user name before the command.
- Issues:
- The script may rely on environment variables that are not set in the minimal cron environment.
- Scripts containing non-text characters can cause failures
Troubleshooting Steps
- Log Script Output: Redirect the script's output to a log file to see any error messages.
-
* * * * * /path/to/your/script.sh >> /var/log/your_script.log 2>&1
- Check Permissions: Use
ls -l /path/to/your/script.sh to verify the script has execute (x) permissions. If not, run chmod +x /path/to/your/script.sh.
- Use Full Paths: In your script, replace relative path commands with their full paths (e.g.,
/bin/grep instead of grep).
- Set Environment Variables: Add
PATH and other necessary variables at the top of your cron entry or script to define the environment.
- Check for Newline: Open
/etc/crontab and ensure there is a new line character after the last command in your entry.
- Verify User Field: For
/etc/crontab, ensure the user field is present (e.g., root).
- Use
cron.d: For root-owned jobs, consider placing them in /etc/cron.d/ instead of directly editing /etc/crontab for better organization
Regards