2177355_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2177355_en-US

2177355_en-US

dpaa2 dpsw port report dpsw_cnt_ing_no_buffer_discard: xxxx error

i want to forwarding udp traffic to vpp via  dpsw port on lx2160a board.

when i generate  1.2Gps udp traffic to dpsw port .
we find the max_rate that dpsw can reach is only 900Mps,

use restool we find dpsw report dpsw_cnt_ing_no_buffer_discard:22262XXX

the dpsw configuration as below:

ls-addsw  -s=32768 -i=4 dpmac.15 dpni.1 dpmac.5 dpni.5
soc:LX2160a
kernel:4.19.90

MC firmware version: 10.38.1

we don't know how to fix it .
Anybody can help us?
best regards

Re: dpaa2 dpsw port report dpsw_cnt_ing_no_buffer_discard: xxxx error

Hello,

Please try to update the firmware:

https://github.com/nxp-qoriq/qoriq-mc-binary

https://community.nxp.com/t5/Layerscape-Knowledge-Base/LX2160ARDB-How-to-update-MC-firmware-DPC-and-...


Regards

Re: dpaa2 dpsw port report dpsw_cnt_ing_no_buffer_discard: xxxx error

The port speed is 10Gbps.
I checked the guide you referred to, but I couldn't find the solution.
Could you please advise on how to resolve this?

Best regards

Re: dpaa2 dpsw port report dpsw_cnt_ing_no_buffer_discard: xxxx error

Hello,

The DPAA2 architecture and its DPSW component are designed to handle high-speed traffic,
but the actual speed will be that of the physical port being used, which can be 1 Gbps,
10 Gbps, 25 Gbps or even higher, depending on the SoC (System-on-Chip) specifications
and configuration.

You can check the setting up ethernet switch capability

https://docs.nxp.com/bundle/Layerscape_Linux_Distribution_POC_User_Guide/page/topics/setting_up_ethe...

https://docs.kernel.org/6.2/networking/device_drivers/ethernet/freescale/dpaa2/switch-driver.html

 

Regards

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 05:45 PM
更新者: