I have downloaded "SW32K1_S32M24x_RTD_4.4_3.0.0_QLP02" RTD driver from NXP.
But i am unable to use it as I am getting "No license for module ....." for all modules.
I checked the plugins folder.
The CRYPTOMANIFESTSIG.MF and CRYPTOMANIFEST.MF files are missing in META-INF folder for all modules.
Does anyone have a solution for this problem ?
Here is the reply from SW team:
After comparation between 3.0.0 QLP02/03 and 3.0.0 version, I saw that: in the 3.0.0 QLP02/03, there are missing files (CRYPTOMANIFEST.MF and CRYPTOMANIFESTSIG.MF) that used to check license.
This caused license issues from the customer's side.
The dev team also detected this issue, they will provide update packages soon.
At the present, there are no workaround and a tentative date. The customer needs to wait for the new packages.
Sorry, let me double-check:
The default RTD path is C:\NXP\SW32K1_S32M24x_RTD_4.4_3.0.0_QLP02
The default path for EBTresos is C:\EB\tresos, and the only file in C:\EB\tresos\links is SW32K1_S32M24x_RTD_4.4_3.0.0_QLP02.link
In addition, MEM_43_INFLSand MEM_43_EXFLScan also be seen in SW32K1_S32M24x_RTD_R21-11_3.0.0_D2503_ReleaseNotes.pdf, but the Plugin name is not FLS in SW32K1_S32M24x_RTD_4.4_3.0.0_QLP02_D2505_ReleaseNotes.pdf.
Do you only want AUTOSAR 4.4 and not AUTOSAR R21-11?
Hi
The reinstall does not solve the issue.
SW32K1_S32M24x_RTD_R21-11_3.0.0_D2503.exe. does not have FLS module. So, we will not be able to use it.
Can we use "SW32K1_S32M24x_RTD_4.4_R21-11_2.0.0_P01" as a temporary solution? What are the differences between these versions - RTD_4.4_R21-11_2.0.0_P01 and RTD_4.4_3.0.0_QLP02_D2505 ?
Hi
Sorry for the inconvenience we bring you!
If you still receive a license error message when reinstall both EB Tresos and SW32K1_S32M24x_RTD_4.4_3.0.0_QLP02_D2505.exe in the default path, you may have to temporarily install SW32K1_S32M24x_RTD_R21-11_3.0.0_D2503.exe.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------