Hello team,
I am trying to create an example using Design Studio 3.6.0 with RTD 6.0.0 QLP1 and specifically when using the Crypto Driver and change the name of the NvmKeyCatalog I start seeing interface issues like the following picture:
Until I get the following error indicating that there was an error in the execution of Javascript.
This only happens when using the Crypto_43_HSE and I hadn't had any issues with Crypto_43_ACE or other peripherals.
Best Regards,
Jesus Cinco
@Jesus_Cinco
I tested again on S32DS 3.6.4, this issue was disapeared
Please try this version S32DS
@Jesus_Cinco
Dev team said that there was a bug reported for that, I'm looking for that bug's info again and will share to you later.
It seems like there're some conditions in the container's name, if you change that name it would raise error.
You should keep the name as default to avoid this bug
Hi Cuong,
It doesn't let me modify anything from that point and the error just keeps popping up.
Best Regards,
Jesus Cinco
Hi @Jesus_Cinco
It looks like the configuration in CryptoKeyElement container is blank.
Please config this container and other error container.
Or you can refer the Crypto example provided along with the RTD 6.0.0 QLP1