2175517_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2175517_en-US

2175517_en-US

imx95 configured camera (gc05a2)

HI NXP

1. Download link for camera setup documentation

2. Where is the issue in the log below?

LinuxRe: imx95 configured camera (gc05a2)

I would suggest you try to use libcamera to test.


export LIBCAMERA_PIPELINES_MATCH_LIST='nxp/neo,imx8-isi,uvcvideo'

gst-launch-1.0 libcamerasrc ! queue ! autovideosink
Re: imx95 configured camera (gc05a2)

HI @danielchen 

    1.I've enabled media linking with the command (media-ctl -d /dev/media0 -l "'gc05a2 1-0037':0 -> 'csidev-4ad30000.csi':0[1]")

Re: imx95 configured camera (gc05a2)

Hi, yrj


For BSP 6.12.20,   I would suggest you refer to i.MX Linux Reference Manual  Rev LF6.12.20_2.0.0.

You need to enable the media Link.

Before using GStreamer, you need to enable the media pipeline link between the sensor and CSI,  

Please check the Linux Reference Manual,  search "media-ctl" for more details.



Re: imx95 configured camera (gc05a2)

HI @danielchen 

       1.BSP:imx-6.12.20-2.0.0.xml

       2.This version is already very new. Is it necessary to use version 6.12.34?




Re: imx95 configured camera (gc05a2)

which BSP version you are using?  can you try the latest BSP version 6.12.34

Re: imx95 configured camera (gc05a2)

HI @danielchen 

     1.Check the formats supported by /dev/video2, in case they do not meet expectations

     2.The format is incorrect; it is suspected that the CSI and the camera are not compatible.

yxjiang_0-1759211343430.pngyxjiang_0-1759211343430.png

Re: imx95 configured camera (gc05a2)

From the log file, the GC05A2 sensor at I2C address 1-0037 is detected and linked to the CSI interface.

gc05a2 1-0037 → csidev-4ad30000.csi → crossbar → mxc_isi.2 → /dev/video2


The format negotiation shows

    • GC05A2 outputs SGRBG10_1X10/2592x1944
    • CSI and ISI are configured for UYVY8_1X16/1920x1080

This implies that format conversion is happening, likely via ISI, and the pipeline is correctly routed to /dev/video2.

Below fail log shows the requested format is not supported by the V4L2 device /dev/ivdeo2

danielchen_0-1759210168607.pngdanielchen_0-1759210168607.png



Re: imx95 configured camera (gc05a2)
Why is there an error in the log?
Re: imx95 configured camera (gc05a2)

Hi @yrj 


I would suggest you refer to UG10215:  i.MX Camera Porting Guide.

https://www.nxp.com.cn/docs/en/user-guide/UG10215.pdf

This document provides an overview of the i..MX95 applications processor hardware camera subsystem, and then describes its corresponding software architecture with the Linux Kernel and User space.  It also describes the porting instructions and how to configure the 3A algorithms.


Regards

Daniel





Regards

Daniel

Tags (1)
No ratings
Version history
Last update:
‎11-22-2025 08:32 AM
Updated by: