Hello everyone,
I wanted to ask how to program ADKP in Base Secure Boot
S32K344-WB #HSE#BaseSecureBoot
Thanks
Hello everyone,
I’m working with an S32K312EVB-Q172 board and I’d like to test the HSE demo examples.
Would it be possible to get access to the file S32K3_HSE_DemoExamples_1_0_0.zip?
I’m using S32 Design Studio for S32 Platform together with a PEMicro debugger.
Thank you in advance for your help!
Best regards,
Davide
I recommend reviewing the following thread, as it may be related to the problem you are experiencing.
Hello,
After successfully booting the bootloader (HSE_SignBootImage OK) and passing the verification, the system displays a brief LED blue flash (indicating a successful Secure Boot). However, upon reboot or a second debug, the system crashes and it does not pass /* Verify that the generated TAG is valid for the APPBL */
#if VERIFY_TAG
srvResponse = HSE_VerifyBootImage(pAppBL);
ASSERT(HSE_SRV_RSP_OK == srvResponse);
I suspect the problem is an overwrite. Do you know how to fix it?
Thank you very much
The HSE service response 0x55A5AA33 corresponds to HSE_SRV_RSP_OK.
However, if you are encountering issues when calling the HSE_SignBootImage() function, I recommend reviewing the following thread, as it may be related to the problem you are experiencing.
HSE_VerifyBootImage return HSE_SRV_RSP_VERIFY_FAILED
If the issue persists or the thread does not address your specific case, please let me know.
I have S32K3_HSE_DemoExamples_1_0_0, S32K344 device
The ADKP is programmed successfully (check_debug_password_programmed_status() returns TRUE).
However, the function HSE_SignBootImage() continues to fail immediately upon invocation, returning the error code 0x55a5aa33
In the main of Basic Secure Boot it does not pass the assert
/* Verify that the generated TAG is valid for the APPBL */
#if VERIFY_TAG
srvResponse = HSE_VerifyBootImage(pAppBL);
ASSERT(HSE_SRV_RSP_OK == srvResponse);
#endif
I generate S32K344_SecureBootBlinky.bin, I put it in C:\NXP while the SecureBootBlinky and the Basic_SecureBoot are in C:\NXP\S32K3_HSE_DemoExamples_1_0_0\S32K3_HSE_DemoExamples\Secure_Boot
I noticed in the linker file of Basic Secure Boot "S32K344_flash.ld" there is not
_adkp_key :
{
. = ALIGN(4);
KEEP(*(_adkp_key))
. = ALIGN(4);
} > PFLASH
Do I have to modify that file? i attach it to you
/*****************************************************************************
*
* Copyright 2020-2022 NXP
* All Rights Reserved
*
*****************************************************************************
*
* THIS SOFTWARE IS PROVIDED BY NXP "AS IS" AND ANY EXPRESSED OR
* IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES
* OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED.
* IN NO EVENT SHALL NXP OR ITS CONTRIBUTORS BE LIABLE FOR ANY DIRECT,
* INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES
* (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR
* SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION)
* HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT,
* STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING
* IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
* THE POSSIBILITY OF SUCH DAMAGE.
*
****************************************************************************/
__STACK_SIZE = 0x00001000;
__HEAP_SIZE = 0x00001000;
/* Linker script to configure memory regions. aggiungi PFLASH_SECURE se vuoi una regione dove mettere chiavi critiche*/
MEMORY
{
ITCM (RWX) : ORIGIN = 0x00000000, LENGTH = 0x10000
PFLASH (RX) : ORIGIN = 0x400000, LENGTH = 0x3f4000
DFLASH (RX) : ORIGIN = 0x10000000, LENGTH = 0x20000
DTCM (RW) : ORIGIN = 0x20000000, LENGTH = 0x20000
SRAM0_STDBY (RW) : ORIGIN = 0x20400000, LENGTH = 0x8000
SRAM (RW) : ORIGIN = 0x20408000, LENGTH = 0x48000
}
/* Linker script to place sections and symbol values. Should be used together
* with other linker script that defines memory regions FLASH and RAM.
* It references following symbols, which must be defined in code:
* Reset_Handler : Entry of reset handler
*
* It defines following symbols, which code can use without definition:
* __exidx_start
* __exidx_end
* __ecc_table_start__
* __ecc_table_end__
* __etext
* __data_start__
* __preinit_array_start
* __preinit_array_end
* __init_array_start
* __init_array_end
* __fini_array_start
* __fini_array_end
* __data_end__
* __bss_start__
* __bss_end__
* __end__
* end
* __HeapLimit
* __StackLimit
* __StackTop
* __stack
*/
ENTRY(Reset_Handler)
SECTIONS
{
.text :
{
KEEP(*(.vectors))
*(.text*)
KEEP(*(.init))
KEEP(*(.fini))
/* .ctors */
*crtbegin.o(.ctors)
*crtbegin?.o(.ctors)
*(EXCLUDE_FILE(*crtend?.o *crtend.o) .ctors)
*(SORT(.ctors.*))
*(.ctors)
/* .dtors */
*crtbegin.o(.dtors)
*crtbegin?.o(.dtors)
*(EXCLUDE_FILE(*crtend?.o *crtend.o) .dtors)
*(SORT(.dtors.*))
*(.dtors)
*(.rodata*)
KEEP(*(.eh_frame*))
} > PFLASH
.ARM.extab :
{
*(.ARM.extab* .gnu.linkonce.armextab.*)
} > PFLASH
__exidx_start = .;
.ARM.exidx :
{
*(.ARM.exidx* .gnu.linkonce.armexidx.*)
} > PFLASH
__exidx_end = .;
.ecc.table :
{
. = ALIGN(4);
__ecc_table_start__ = .;
QUAD (__data_start__)
QUAD ((__data_end__ - __data_start__) /
QUAD (__bss_start__)
QUAD ((__bss_end__ - __bss_start__) /
QUAD (__HeapTop)
QUAD ((__HeapLimit - __HeapTop) /
QUAD (__StackLimit)
QUAD ((__StackTop - __StackLimit) /
QUAD (ORIGIN(ITCM))
QUAD (LENGTH(ITCM) /
QUAD (ORIGIN(DTCM))
QUAD (LENGTH(DTCM) /
__ecc_table_end__ = .;
} > PFLASH
.copy.table :
{
. = ALIGN(4);
__copy_table_start__ = .;
LONG (__etext)
LONG (__data_start__)
LONG ((__data_end__ - __data_start__) / 4)
/* Add each additional data section here */
/*
LONG (__etext2)
LONG (__data2_start__)
LONG ((__data2_end__ - __data2_start__) / 4)
*/
__copy_table_end__ = .;
} > PFLASH
.zero.table :
{
. = ALIGN(4);
__zero_table_start__ = .;
/* Add each additional bss section here */
/*
LONG (__bss2_start__)
LONG ((__bss2_end__ - __bss2_start__) / 4)
*/
__zero_table_end__ = .;
} > PFLASH
__etext = ALIGN(8);
.boot_header :
{
KEEP(*(.boot_header))
} > DFLASH
.standby_ram :
{
*(.standby_ram)
} > SRAM0_STDBY
/* Due ECC initialization sequence __data_start__ and __data_end__ should be aligned on 8 bytes */
.data : AT (__etext)
{
. = ALIGN(8);
__data_start__ = .;
*(vtable)
*(.data)
*(.data.*)
. = ALIGN(4);
/* preinit data */
PROVIDE_HIDDEN (__preinit_array_start = .);
KEEP(*(.preinit_array))
PROVIDE_HIDDEN (__preinit_array_end = .);
. = ALIGN(4);
/* init data */
PROVIDE_HIDDEN (__init_array_start = .);
KEEP(*(SORT(.init_array.*)))
KEEP(*(.init_array))
PROVIDE_HIDDEN (__init_array_end = .);
. = ALIGN(4);
/* finit data */
PROVIDE_HIDDEN (__fini_array_start = .);
KEEP(*(SORT(.fini_array.*)))
KEEP(*(.fini_array))
PROVIDE_HIDDEN (__fini_array_end = .);
KEEP(*(.jcr*))
. = ALIGN(8);
/* All data end */
__data_end__ = .;
} > SRAM
/* Due ECC initialization sequence __bss_start__ and __bss_end__ should be aligned on 8 bytes */
.bss :
{
. = ALIGN(8);
__bss_start__ = .;
*(.bss)
*(.bss.*)
*(COMMON)
. = ALIGN(8);
__bss_end__ = .;
} > SRAM
/* Due ECC initialization sequence __HeapTop and __HeapLimit should be aligned on 8 bytes */
.heap (COPY):
{
. = ALIGN(8);
__HeapTop = .;
__end__ = .;
_end = .;
PROVIDE(end = .);
. = . + __HEAP_SIZE;
. = ALIGN(8);
__HeapLimit = .;
} > SRAM
/* Due ECC initialization sequence __StackLimit and __StackTop should be aligned on 8 bytes */
.stack (ORIGIN(SRAM) + LENGTH(SRAM) - __STACK_SIZE) (COPY) :
{
. = ALIGN(8);
__StackLimit = .;
. = . + __STACK_SIZE;
. = ALIGN(8);
__StackTop = .;
} > SRAM
PROVIDE(__stack = __StackTop);
/* Check if data + heap + stack exceeds RAM limit */
ASSERT(__StackLimit >= __HeapLimit, "region RAM overflowed with stack")
CM7_START_ADDRESS = ORIGIN(PFLASH);
__STDBYRAM_START = ORIGIN(SRAM0_STDBY);
__STDBYRAM_SIZE = LENGTH(SRAM0_STDBY);
}
Refer to the following thread, which contains information related to this topic and may be helpful for you.
[S32K3] Restrict the debug access with a password when HSE is used
Additionally, I recommend reviewing the implementation of the functions ProgramADKPService(), Advance_LifeCycle_Service(), and attributeProgrammingService() provided in the S32K3 MCUs for General Purpose HSE Demo Examples and/or the HSE_DEMOAPP.
BR, VaneB