2173493_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2173493_en-US

2173493_en-US

PN7642 - Initial Calibration

Hello Community,

i have a custom PCB with PN7642.

The Datasheet says, that before turning on the RF part, an initial calibration needs to be done.

Is there any further documentation about this than:

1. Write EEPROM configuration NOV_CFG_CAL.
2. Write REGISTER TX_NOV_CALIBRATE_AND_STORE_VAL_REG.
3. Write EEPROM configuration NOV_CFG_CAL.?

Which values should be set?

Thank for helping.


Best regards

Oliver

Re: PN7642 - Initial Calibration

Hello @MPEngineering 

This part should be encapsulated, and recommends to run the project:

PN7642_MCUXpresso_SDK_02-15-003_PUB\boards\pnev7642fama\nfc_examples\pub\NFC_Config, and select "RFLD_NFCLD_CONFIG"

KaiLi_0-1758693133679.pngKaiLi_0-1758693133679.png

After that, the device can be initialized and calibrated.

Re: PN7642 - Initial Calibration

Hey @KaiLi ,

thanks for replying.

Yes, i have the SDK. So with flashing an example its calibrated?
I looked for the definitions of the Registers in some examples and also in the API Reference Manual. 
I don´t see them. 

Maybe my question was a bit unclear.
I want to know, what i have to write into REGISTER TX_NOV_CALIBRATE_AND_STORE_VAL_REG.
Cause there is no further explanation. Its 2 bit r/w register. What happens if i write 0x1, 0x2 or 0x3 into it?

NOV_CONFIG_CAL is clear. First write 0x01 for cold boot FW calibration and after succesfull calibration write 0x02 to reference to NOV_CAL_VAL1 and 2.


Best regards

Oliver

Re: PN7642 - Initial Calibration

Hello @MPEngineering 

It's recommended that you can run SDK the example

log in:

Best-in-Class NFC Frontend with Integrated MCU | NXP Semiconductors

and download:

KaiLi_0-1758595034002.pngKaiLi_0-1758595034002.png


タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 11:30 PM
更新者: