2170199_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2170199_en-US

2170199_en-US

HDMI Interface is not working in I.MX8QM Evaluation Board.

Hi,

HDMI Interface is not working in I.MX8QM Evaluation Board and all other interfaces are working

Previously HDMI interface worked properly, and we are using same previous SD card and Board booting through SD card.

Now Issue Showing as "cdns-mhdp-imx 56268000.hdmi: Falling back to sysfs fallback for hdmitxfw.bin".

Please help us to resolve this Issue.

Re: HDMI Interface is not working in I.MX8QM Evaluation Board.

The i.MX8 QM provides an HDMI transmitter capable of supporting an HDMI2.0 compatible output, a Display Port 1.3 compatible output, or an embedded Display Port 1.4 compatible output. 

Here which version BSP are you using? Are you using the demo images or the images you build youself? 

The firmware file hdmitxfw.bin should be present in /lib/firmware/.

 

On yur board, run:

ls /lib/firmware/hdmitxfw.bin
If the file is missing, that’s the root cause.
 

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 06:32 AM
Updated by: