2169480_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2169480_en-US

2169480_en-US

How to display AR0144 Stream without waveshare 7 inch lcd in Zephyr Os

    there are a IMX93_EVK board a AR0144 sensor , want to develop AR0144 with Zephyr OS in IMX93_EVK .

    found a example about  camera_demo with AR0144 in FRDM_IMX93 : Run Zephyr on A55 with FRDM-IMX93 and FRDM-IMX91  .

    could refer from this sample .  but it may need waveshare-7-inch-lcd to show the stream . 

   wanna know how to display AP0144 stream without the 7 inch lcd ? or whether there is a interface for IMX93_EVK  to connect with monitor by HDMI or any other devices to show stream from AR0144 .

    Appreciate your help . 

Re: How to display AR0144 Stream without waveshare 7 inch lcd in Zephyr Os

Hi @Chavira ,

    Thanks for your reply .

    I couldn't get much more information from NXP Forums , I think there was ever someone also ask the same issue ,but NXP couldn't provide more support for Zephyr .

    imx93evk zephyr flashing jlink said : "Unfortunately, this support channel does not provide support for Zephyr.

    Maybe NXP could also update or integrate the AR0144 Zephyr sample from FRDM_IMX93 to IMX93_EVK board  and provide much more support for Zephyr . 

    Thanks !

Re: How to display AR0144 Stream without waveshare 7 inch lcd in Zephyr Os

Hi @workholic365!

Thank you for contacting NXP Support!


Unfortunately, we don’t currently have an example available for the feature you’re looking to implement.


It should be possible to achieve, but you would need to develop it on your side using our existing examples as a reference.


Best regards,
Chavira

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 11:32 PM
更新者: