Hi,
I am working on the MIMXRT1176 and I need to implement BLE with both Central and Peripheral roles along with GATT and GAP profiles. Could you please suggest which example project from the NXP SDK would be the best starting point for this implementation?
Thanks,
Amarnath.
Hi, @Amarnath_473
Thanks for your reply.
Please do not hesitate to mark my answer as an accept solution for this case so that we can close this current thread.
And also, please feel free to create new case to us if you meet any issue when using our product.
Best regards,
Christine.
Hi @Christine_Li,
Thank you for sharing the link and guidance. I will go through the examples. This is very helpful.
Best regards,
Amarnath
Hi, @Amarnath_473
In the SDK release, we have some examples for Central role, and also we have some examples for peripheral role. And I believe below link is really helpful for you to better understand these examples.
You can choose any one according to your requirement.
For each example, it includes detailed explanation and how to use it.
You can configure one of your board as central and another board as peripheral role, so that two boards can communicate with each other.
Best regards,
Christine.
Hi @Gavin_Jia,
Thanks for the suggestions. I am planning to connect an external BLE module (u-blox Maya W4 which is based on IW610) and want to implement GATT and GAP profiles using that module. Could you please suggest any SDK examples or demos that would be suitable for integrating the Maya W4 with RT1176?
Best regards,
Amarnath
Hi @Amarnath_473 ,
Thanks for your interest in NXP MIMXRT series!
The RT1170 itself does not have BLE functionality and requires an external BLE-enabled chip, such as the IW612/RW612 or others.
You can start with these examples: https://github.com/nxp-appcodehub/dm-ble-throughput-measurement-rt1170 and wifi_cli_over_ble_wu demo in RT1170-EVKB SDK.
Best regards,
Gavin