2167024_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2167024_en-US

2167024_en-US

SPC5777CCMMO3 pin out reading eepron

IMG_7633.pngIMG_7633.png

What is the pinout to be able to read the eeprom of this micro with the reader?

3155ac18-7996-4a1a-bf47-f749ef4e56dd.jpeg3155ac18-7996-4a1a-bf47-f749ef4e56dd.jpeg

Re: SPC5777CCMMO3 pin out reading eepron

Hello,

If the micro is censored, you won't be able to connect to flash without 256-bit censorship password.

So trying to connect without valid secure keys is just waste of time, as there are additional protection mechanisms like PASS, and CSE.

Its not like it used to be in old days, uC has now advance secure features to prevent unauthorized accesses.

Best regards,
Peter

Re: SPC5777CCMMO3 pin out reading eepron

Thanks, what I'm looking for is to read the internal flash to be able to remove an anti-tunig block that doesn't allow writing modified files, only writing the original.

Re: SPC5777CCMMO3 pin out reading eepron

Hello,

The pins are described in IOMUX table as I have mention before:

petervlna_0-1757661184211.pngpetervlna_0-1757661184211.png

But I am not sure what your intention is. You will need a JTAG properly connect, like it is on evaluation board in order to work.

Also if the device is censored you need correct password to unlock its flash. Without it you cannot connect to the device at all.

Best regards,

Peter


Re: SPC5777CCMMO3 pin out reading eepron

Hi yes try  reading flash via JTAG. The micro is good. I removed it so I could track and locate where each pin went on the board, and mark points for reading and writing, without having to remove it.

Re: SPC5777CCMMO3 pin out reading eepron

Hello,

Not sure what your intention is, but the pins are explained in IOMUx table attached to reference manul:

https://www.nxp.com/webapp/Download?colCode=MPC5777CRM

You are probably speaking about reading flash via JTAG.

I am confused as your micro looks damaged. So no read of flash is possible if the micro is not working.

Best regards,

Peter

Re: SPC5777CCMMO3 pin out reading eepron

where to buy this 256-bit censorship password.

Tags (1)
No ratings
Version history
Last update:
3 weeks ago
Updated by: