Dear all,
I’ve been trying to run the PDK Uart demo on the
S32Z2 S32Z280-400 EVB board. So far, the configuration and build went smoothly, no errors at all.
But I hit a little snag: when I launch the demo with the NXP Debug probe, the app itself starts up fine, but there’s no output at all on the serial console. I even tried typing “Hello” into the console to test the interaction, and the app didn’t respond either.
Wondering if anyone here has run into a similar issue, or if you have any troubleshooting tips I could try?
Quick heads-up on my setup: I’m using S32 Design Studio 3.6.2, and the board’s connected to my PC directly with a USB-A cable.
Thanks a ton for your help!
Hi,BingBai_S
Thank you for your reply.
Do you use the demo of Uart_Example_S32Z2XX_R52?
BR
Joey
I use S32Z/E PDK version 3.6.0, meanwhile I have tested the semihosting functions, not output anything, when I try to printf() something.
hi,BingBai_S
Which version of RTD are you using? and are you using the demo of Uart_Example_S32Z2XX_R52 ?
BR
Joey