2165977_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2165977_en-US

2165977_en-US

imx8mp Chromium (Ozone/Wayland) on BSP 6.6.23 does not receive input events in RDP session

I am using NXP BSP version 6.6.23 on i.MX8MP with Weston as the Wayland compositor and Chromium 117 built with Ozone/Wayland support.
I have configured a remote desktop session using Weston’s RDP backend. The RDP connection works correctly, and the Chromium window is displayed as expected.
However, Chromium does not receive keyboard or mouse events from the RDP client.
Other applications, such as weston-terminal, work fine in the same RDP session and accept input events without issues.
This problem only affects Chromium when running in the RDP session; locally on DRM output, Chromium works as expected.

Any suggestions or known workarounds for enabling input events in Chromium under Weston RDP sessions?

i.MX 8 Family | i.MX 8QuadMax (8QM) | 8QuadPlusi.MX 8M | i.MX 8M Mini | i.MX 8M NanoRe: imx8mp Chromium (Ozone/Wayland) on BSP 6.6.23 does not receive input events in RDP sessionHi Manuel,

Thanks again for your help. I’ve adapted the patch to Chromium 117 and it’s working great, keyboard and mouse input are now correctly received in the RDP session with Weston.

Really appreciate the support!

Best,
Diego
Re: imx8mp Chromium (Ozone/Wayland) on BSP 6.6.23 does not receive input events in RDP session

Hello @diegoperez 

I hope you are doing very well.


You can try adding the patch shared here.


Best regards,

Salas.

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 12:00 AM
更新者: